Vention's Blog

Blog / #how_to_guides

How-to-Guide - Troubleshooting Linear Axis Direction

Michel Launier AUTOMATION SOFTWARE LEAD / Jan 11th, 2019

Motor Moves in Only One Direction

This blog discusses a problem with the motor moving in one direction but not the other.

There are 3 possible causes for a motor connected to the MachineMotion controller to move in one direction (clockwise/counterclockwise) but not the other.

  1. A missing or defective end-stop sensor
  2. Inappropriate homing of the axis
  3. Defective hardware

Missing or Defective End-Stop

The objective of the end-stops is to constrain the movement on the axis. For safety reasons, a disconnected or defective end-stop is interpreted by MachineMotion as an indication of the end of the axis. Therefore, the controller will not allow any movement in the direction towards the missing or defective end-stop.

vention-single-axis-sensor-normal

Figure 1. Sensors positions in normal axis mode



vention-single-axis-sensor-reverse

Figure 2. Sensors positions in reverse axis mode



vention-machine-motion-face

Figure 3. MachineMotion end-stop sensor connectors



Homing Not Completed Properly

MachineMotion maintains the position of the linear axis internally. This position is initialized by a proper homing operation. If the homing position is not properly initialized, MachineMotion may not allow movement in the negative direction. If the homing position is wrongly set, movement in the negative direction beyond the homing point is prevented by the system.

vention-single-axis-homing

Figure 4. Single Axis homing



Inaproppriate homing can be caused by:

  1. a disconnected or defective end-stop sensor;
  2. a system that did not perform homing

Defective Hardware

The motors are controlled with the following 3 signals:

  • enable => (used to energize the motor)
  • step => (to ask the motor to move by a single step/micro-step)
  • direction => (to control the motor direction clockwise or counterclockwise)
enable
step
direction
Motion Controller
Motor Driver
Motor

Figure 5. Step motor internal hardware connections



A defective connection for the direction signal would cause any movement to always be done in the same direction. That is, both positive and negative movement with interpreted as either always positive or always negative.

Note that this type of defect is improbable and is not analyzed in the troubleshooting flowchart.

Troubleshooting Flowchart for Axis Moving in Only One Direction

To troubleshoot, you will need to access the Control Center application included in every MachineMotion controller. Perform the following steps to launch the 1-axis application:

  1. Connect the USB cable of MachineMotion to your PC (or MAC);
  2. Open your browser and type the following in the URL field:
    1. 192.168.7.2:8888 for Windows and Linux computers
    2. 192.168.6.2:8888 for Mac (OSX) computers
  3. Run the "1-Axis Linear Motion" application

The trouble shooting example discusses a 1-axis system. Multi-axis system can be trouble shoot similarly using the 2 or 3 axes application.

Activate the control center using your Web browser


vention-activate-control-center



Launch 1-axis application

vention-activate-1-axis-app



Use the Home button


vention-homing


Move the axis using the application


vention-move-axis



Troubleshooting Flowchart


Not Connected
Yes
No
Connected
Yes
Yes
No
No
Yes
No
Homing
doesn't stop
Yes
No
Troubleshoot
motor moves in only one direction
Verify
that both
end-stops are
connected?
Perform homing
Test move in
positive then negative
direction
Does motor
move in both
directions?
Resolved
Swap sensor 1A & 1B
Is the
problem on
the reverse
direction?
You have a defective sensor
Disconnect sensor 1A
Move motor in the working direction
Did the
motor move?
Sensor 1A is defective
Sensor 1B is defective
Order new
end-stop sensor
You have a homing or H/W issue
Swap sensors 1A & 1B
to their original position
Power cycle the
Machine Motion
controller
Perform homing
Is homing working?
Test positive
& negative movement
Call Vention
for support
Swap sensor 1A & 1B
Is problem resolved?
Resolved

Comments (0)