Vention's Blog

Blog / #tech

Calculating the Stability of your Cobot Stand

How to make sure that your cobot won’t fall over!

Marc-Andre Kyer Application Engineer / Dec 13th, 2018

Collaborative robots, such as Universal Robots, have become an integral part of many manufacturing processes. Both modular and highly customizable, this technology can be adapted to an increasingly widening range of engineering and manufacturing applications. While the technology itself is largely “plug and play”, the design of a stand or pedestal remains relatively labour-intensive and tends to be unique to each user’s application. Based on intended application, the force, weight, and reach of a robot can vary widely and this must be accounted for in the specific stand design. There exists a few standard open-source stands in Vention’s public assembly library, but individual verification must be performed against the intended use case. This article will walk through key steps to verify the stability of your robot stand.


Stability Verification

Two major factors must be considered when assessing the stability of an object – its base width, and the height of its centre of mass. Specifically with respect to robot stands, it is often necessary to add extra weight near the base of the stand, or increase the stand base width, in order to counteract the weight of the robot, its payload and the powerful motor torque at the base. An assessment routine for the general case of a rolling stand and robot assembly is outlined below. For further advice and project-specific insight, the Vention Applications Engineering team can perform Design Reviews based on their experience and lessons learned.


Calculation Methodology

In calculating robot stand stability, as introduced above, it is important to consider the weight, force, and reach of your robot. In the general case, the stand should be designed for the maximum capacity of the robot at maximum payload, reach, and torque – the maximum loading condition that the stand could be required to withstand. Some users, however, may wish to design a stand to meet application-specific requirements in order to minimize costs. An overview of the calculations required to verify stand stability will be outlined in this section. It is important to note that for this article, all components are assumed rigid. Therefore, deformation under applied load of any component is not considered. This topic will be addressed in a future article.


The necessary calculations will be illustrated via assessment of the following assembly:


Figure 1: Robot and stand assembly. Note that center of mass has already been designated for each component. For the robot, we assume the center of mass to occur at 50% of the robot’s arm reach, at point R/2.

1. First, calculate the center of mass for both stand and robot.

2. Two Free-Body Diagrams must now be constructed – for the stand, and for the robot.

a. The robot’s Free-Body Diagram must include forces acting due to the payload weight at maximum reach, and the robot weight (assumed to act at 50% reach, as shown above). These will be used to calculate the reaction forces (torque and vertical force) acting on the mounting plate that secures the robot to the stand.

 

Known Values:
TM = max torque by robot's base joint [Nm]
mPL = max robot payload [kg]
mR = mass of robot [kg]
R = robot reach [m]
g = gravity, 9.81 [m/s2]

Unknown Values:
TB = robot base plate reaction torque [Nm]
Fz = robot base plate reaction force [N]

Figure 2: Free Body Diagram of robot. Here, black arrows denote the forces and moments generated due to both the robot's weight and operating payloads. We must calculate TB and Fz, the torque and reaction force generated at the robot mounting plate.

 

b. The stand’s Free-Body Diagram must include the stand weight, normal force on each wheel (or ground contact point) of the stand and the reaction forces calculated above for the robot’s mounting plate.


Known Values:
ms = mass of stand [kg]
g = gravity, 9.81 [m/s2]
TB = robot base plate reaction torque [Nm]
Fz = robot base plate reaction force [N]
S = stand center of gravity position [m]
dR = distance btw robot base and stand POC with floor [m]
L = lenght of the stand

Unknown Values:
FF = floor front POC reaction force

Figure 3: Free Body Diagram of stand. Note that the force and torque from the robot FBD are included here. In subsequent steps, we will calculate FF

 

3. We now calculate the reaction forces in the robot FBD. We find the vertical components of the robot’s weight forces, via the equation:

ΣVertical Forces = 0
FZ = mPL * g + mR * g

Then, we sum moments acting on the robot base plate – these are due to robot max torque TM and the weight forces of the arm. The equation in this case is:

Σmoments relative to center of robot base = 0
TB = TM + mPL * g * R + mR * g * R/2

4. Finally, we sum moments acting on the stand as outlines in its FBD to determine the reaction forces at its points of contact with the ground. This is achieved for our example by summing the weight force of the stand, the torque due to the robot’s weight, the robot max base torque, and the torque due to the robot payload, as follows:

Σmoments relative to back POC = 0
0 = m S * g * S + F Z * d R - T B - F F * L
F F = (m S * g * S + F Z * d R - T B) / L

5. If reaction forces (here, FF) are greater than zero, then the stand is stable. If not, the stand is unstable.

6. If unstable, design changes must be made. Options include adding weight to the stand, or increasing its base width. Here, a Design Review from Vention’s Applications Engineering Team is a great resource - they can propose design modifications based on their extensive experience.


Calculations


To show an example of these calculations we have selected a Vention Official design for a Universal Robots mobile workstation.

UR3e Heavy-Duty Mobile Workstation



Considering the worst case scenario:


TM = 56Nm

mPL = 3kg
mR = 11kg
R = 0.500m
g = 9.81 m/s2
 
ΣVertical Force = 0
FZ = mPL * g + mR * g 
FZ = 3 * 9.81 + 11 * 9.81 
FZ≅ 140 N
 
Σmoments relative to center of robot base = 0
TB = TM + mPL * g * R + mR * g * R/2  
TB = 56 + 3 * 9.81 * 0.50 + 11 * 9.81 * 0.500 / 2
TB≅100Nm


ms = 45kg
g = 9.81 m/s2
TB = 140Nm
Fz = 100N
S = 0.370m
dR = 0.045m
L = 0.765m
 
Σmoments relative to back POC=0
0=mS * g * S + FZ * dR-TB-FF * L
FF= (mS * g * S + FZ * dR-TB) / L
FF=(45 * 9.81 * 0.370 + 140 * 0.045-100) / 0.765
FF≅91N

FF≥0
The Stand is stable


To optimize for a shorter stand
*Assuming that S is approximately equal to L/2
 
FF =  (mS * g * L/2 + FZ * dR-TB) / L
0 = (45 * 9.81 * Lmin/2 + 140 * 0.045-100) / Lmin
-45 * 9.81 * Lmin/2 = 140 * 0.045-100
Lmin = 2 * (140 * 0.045-100) / (-45 * 9.81)
Lmin = 0.425m
 
Then we can find the Safety Factor
SF = L / Lmin
SF = 0.765 / 0.425
SF = 1.8



Conclusion

Robot arms require structured environments to operate: they need a rigid base for support and effective fixturing for its workspace and tools. Another critical design consideration is to guarantee the stability of the overall assembly. As described in this article, both gravity and motor torques need to be considered. By understanding the various parameters that make stands unstable, designers can engineer their assemblies and optimize for both safety and cost.




Comments (0)